• Registrering
  • Login

Nyhetscenter

Print page

Robotar

Få tillgång till originalkällor

Senaste nytt

2018-11-29 – Automation trends in the packaging industry

Like many other industries, the packaging sector constantly adapts to market requirements. Changes are being influenced by factors such as regulation, skills shortages and digital transformation. To turn these challenges into opportunities, innovative companies are increasingly relying on solutions such as human-robot collaboration and the use of artificial intelligence to ...

Robotar

2018-11-28 – Holistic Solutions for Smart Manufacturing

As digitalization, Big Data and the Industrial Internet of Things (IIoT) take their course, the classical linear manufacturing model is changing: Complex, integrated networks are developing that aim to achieve higher productivity with lower resource consumption. Machines, devices and applications must become smarter accordingly. When it comes to investment decisions, cooperation with ...

2018-08-14 – Industrial robots are on the move

An autonomously guided vehicle (AGV) equipped with a robot arm from Mitsubishi Electric is making it possible to deploy the same robot at multiple workstations. The system has been designed to provide flexibility on assembly lines and boost plant productivity.

2018-07-31 – Faster start-up with new MELFA FR robot series

Mitsubishi Electric’s new industrial robot series combines reduced cycle times with scalable safety features and offers versatile connectivity options for easy integration into production systems. Companies who want to achieve a more flexible and productive working environment will also benefit from new capabilities created by the implementation of artificial intelligence.

2017-11-29 – Mitsubishi Electric previews extension to its range with collaborative robot

Supporting humans with a full complement of robot features and equipment on board At SPS IPC Drives from 28 - 30 November 2017 in Nuremberg, Mitsubishi Electric is setting up a demonstration of production in an Industry 4.0 environment that will include a new collaborative robot, working together with an operator without safety barriers.

2017-09-20 – Debut at EMO 2017 - New concept in robotics for predictive maintenance

EMO Hannover 2017, 18th – 23rd September 2017, Hannover, Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is using EMO 2017 to demonstrate innovative predictive maintenance possibilities for robots that can reduce operational costs, increase asset productivity and improve process efficiency. The cloud-based solution is based on the AI platform within IBM Watson, which enables ...

2017-09-18 – Solutions for the digital transformation of production

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 In an increasingly competitive manufacturing environment, businesses need flexibility, improved productivity, and the capability to make gains in efficiency and reductions in downtime. Mitsubishi Electric is showing how these requirements can be met with a focus on connected production systems....

2017-08-21 – Mitsubishi Electric delivers solutions for digital transformation at EMO 2017

At the EMO exhibition in Hannover, visitors to Mitsubishi Electric’s stands can experience how to benefit from ongoing digitalisation at a manufacturing level. The theme “e F@ctory – pushing business further” covers a wide range of technologies aligned to current challenges in the machine building sector.

2017-07-25 – A Lion for three robots

Mitsubishi Electric’s interactive robotic installation known as “Threebots” has been awarded with the coveted Silver Lion in Cannes. “Threebots” has already received several awards since its installation at the German branch in Ratingen.

2017-05-05 – Key technology supporting packaging applications on their journey to Industry 4.0

Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017.

2017-04-24 – SAP, Mitsubishi Electric Enable New IoT-Based Services for Manufacturing with SAP® Cloud Platform

SAP SE (NYSE: SAP) and Mitsubishi Electric Europe today announced SAP’s participation in Mitsubishi Electric e-F@ctory Alliance partner program. This partnership will enable Mitsubishi Electric’s automation solutions to operate fully with SAP® Cloud Platform...

2016-12-13 – Mitsubishi Electric’s “Threebots” honoured with Red Dot Design Awards

In November, Mitsubishi Electric was presented with the “Best of the Best” and “Grand Prix 2016” awards at the prestigious Red Dot Gala. The prizes were awarded for the interactive “Threebots” robot application which can be found at the company’s German branch in Ratingen.

2016-10-31 – Solutions for Industry 4.0 presented by Mitsubishi Electric at SPS IPC Drives 2016

At the forthcoming SPS IPC Drives Expo Mitsubishi Electric is showcasing a portfolio of integrated automation components and services developed to help customers realise their individual business objectives. Visitors to this year’s booth can explore new application solutions that enable the automation and digitalization of industrial processes and also exchange ideas ...

2016-09-06 – Mitsubishi Electric’s ‘Threebots’ Interactive Robot Installation Receives Several Awards

Mitsubishi Electric’s interactive robotic installation known as ‘Threebots’ has received several coveted awards since its installation at the new German branch office in Ratingen. They include the ‘Cutting Edge Award’ presented by Adobe, and ‘FWA’ (thefwa.com) the latter of which was awarded by a jury of more than 200 experts in recognition of projects that use cutting-edge technology to ...

2016-03-17 – New - Mitsubishi Electric powered Delta robots from Codian Robotics

Mitsubishi Electric’s popular MELFA range of compact SCARA and articulated arm robots has been effectively extended by the introduction of new Delta style robots from well-known manufacturer Codian Robotics. Employing high precision servo motion technology and easy to use software from Mitsubishi Electric the new range is fast, precise and user friendly. Ideal for lightweight pick-and-place...

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-08 – Mitsubishi Electric announces a significant presence at UK Drives & Controls fair, 2016

UK trade shows have experienced their ups and downs over the last two or three decades, however, they have endured and are now enjoying somewhat of a resurgence in popularity as exhibition organisers and venues work together to improve the relevance and accessibility of their events. Against this backdrop Mitsubishi Electric has committed to take a large space at the 2016 Drives & Controls ...

2015-11-27 – Safer and more productive interaction between humans and robots enabled by MELFA SafePlus and safety sensor technology

At SPS IPC Drives 2015, Mitsubishi Electric, together with its system partner MH Elektro-Steuerungstechnik, are presenting an industrial robot that enables humans and robots to work together more safely and effectively during large batch production within closely confined work cells. In order to do that, an industrial robot from the MELFA F series of Mitsubishi Electric has been equipped with...

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-07-30 – Industry 4.0 in the Food and Beverage industry

The practical advantages that the new cyber-physical interface of Industry 4.0 brings are acknowledged by engineers across a range of industries. Jeremy Shinton, Product Manager UK – Business Solutions at Mitsubishi Electric Europe B.V., UK Branch, Automation Systems Division, explains how food and drink manufacturers in particular can benefit from the implementation of Industry 4.0:

2015-04-28 – “MELFA SafePlus” enables robots and humans work together in harmony

Mitsubishi Electric has developed a new optional Safety Solution “MELFA SafePlus” for its MELFA F Series industrial robots. The new technology limits the speed, range of movement or torque of the robot when safety sensors are activated, allowing operators to work in close proximity to a moving robot.

2015-04-16 – Mitsubishi Electric and partners demonstrate hands-on handling solutions

At this year's Hannover Messe, Mitsubishi Electric and partners will be presenting hands-on handling and automation solutions. The focus will be on robotics including an integrated high-precision, flexible laser marking solution from Taufenbach GmbH, an automated screw application system from WSM-Automation GmbH, an application from Bilfinger HSG and Datalogic S.R.L. ...

2015-03-02 – Preview Anuga - Complete solutions for the food and beverage industry from a single source

As a supplier of complete solutions, Mitsubishi Electric will be exhibiting its comprehensive range of products designed especially for the food and beverage industry at Anuga FoodTec in Hall 07.1, Stand A109. Visitors to the stand will also be able to witness the high-speed performance of the latest RH-F series overhead SCARA robot as it carries out a typical pick-and-place application....

2014-10-10 – Mitsubishi Electric and Robotronic present highly compact handling solution for ready-to-use syringes

At Motek trade fair 2014, Mitsubishi Electric Europe and robotics specialist Robotronic will be demonstrating the world's first handling concept for supplying ready-to-use syringes to an end-of-line packing system. The solution concept is exceptionally compact and extremely fast with a processing rate of up to 600 syringes per minute. It is also so flexible that easy switching between different...

2014-08-19 – MELFA-3D Vision and Sensor-less Servo Win R&D 100 Awards

Mitsubishi Electric Corporation (TOKYO: 6503) announced today that two of its factory-automation technologies, MELFA-3D Vision and Sensor-less Servo, have each won a 2014 R&D 100 Award from R&D Magazine. The awards, commonly known as the “Oscars of Innovation,” underline Mitsubishi Electric’s continuing status as a global leader in industrial innovation.

2014-05-15 – Making baked products manufacturing fit for the future: Productivity and efficiency through data transparency

Pressure on prices is rising in the bakery market. Of particular concern is the increasing pressure from the discounters who are competing with cheap products baked freshly in store. At the same time, productivity and profit margins are low in the food processing industry in comparison to other producing industries. Above all ...

2014-04-22 – Preview components 2014 - Mitsubishi Electric Europe and Robotronic exhibit world’s first syringe handling solution with a small footprint

At this year’s components show, which is being staged in parallel with interpack, Mitsubishi Electric Europe and Swiss robotics specialist Robotronic are jointly presenting a brand new handling solution for supplying pre-filled syringes to an end-of-line packing system. The unique concept takes up very little space, yet offers a high processing rate of up to 600 syringes per minute and ...

2014-02-06 – Making bakery production future-ready thanks to data transparency

At this year’s trade press days in Karlsruhe, Mitsubishi Electric is switching the focus to the bakery industry with its presentation “Increasing Productivity through Automation Technology in the Food Industry”. Stefan Knauf, Corporate Account Manager Food & Beverage, CPG, at Mitsubishi Electric’s Factory Automation – European Business Group, will look at options for improving efficiency...

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-26 – 3D-based robot technology: Adaptive handling for Mitsubishi Electric robots

Visitors to the Mitsubishi Electric stand (Hall 7, Stand 380) at this year’s SPS IPC Drives will be able to experience live the latest developments in the field of 3D-based robotics. Mitsubishi Electric, along with partner isys vision GmbH, will be presenting the RoboView 3D stereo vision system that allows adaptive handling by MELFA robots. For the trade fair, the system has been integrated in ..

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-11-07 – Mitsubishi Electric’s iQ Platform: full automation on one rack

Machine tool manufacturers have been successfully combining Mitsubishi Electric CNC and robot technology in their systems for years and consequently promoting unmanned production. The iQ Platform from Mitsubishi Electric permits not only the seamless combination of CNC and robot CPUs but also of PLC and Motion Control CPUs – an integrated solution that is unique throughout the industry...

2013-06-13 – Mitsubishi Electric sponsors WorldSkills Leipzig 2013

1000 trainees and skilled workers, 67 countries and regions, 46 official competitive disciplines, 200,000 visitors, 3000 specialists, 1000 journalists and 38 robots from Mitsubishi Electric – this is the vocational World Cup. From 2 to 7 July, the best skilled workers in the world will be competing at the WorldSkills Leipzig 2013 event by demonstrating their abilities in a wide variety of ...

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2012-12-04 – Combat rising energy costs with energy management systems from Mitsubishi Electric

Energy transition has resulted in an increase in energy costs and has made the subject of energy efficiency increasingly significant. The primary concerns of the production industry include the need to ensure that companies remain competitive, even with rising energy costs, and that production processes continue to run smoothly without any problems.

2012-09-14 – Mitsubishi Electric brings automation to baking technology and optimises production efficiency

This year, for the first time, Mitsubishi Electric – a long-term baking technology partner – will have its own stand at the iba trade fair to be held in Munich from 16-21 September 2012. The company will be presenting its comprehensive range of automation components for bakeries on stand 135 in hall B4. The highlight of the stand will be an interactive live application.

2012-04-25 – Mitsubishi Electric sets new performance benchmarks with F Series SCARA robots

Mitsubishi Electric has extended its RH range of MELFA SCARA robots with the launch of the new F Series, setting new benchmark standards for speed, flexibility, ease of integration and simplicity of programming. Combining a wide area of coverage with the industry’s fastest cycle times, the F Series provides a cost-effective means to boost productivity on critical production lines.

2012-03-13 – Precision robot cell for the pharmaceutical industry uses automation technology from Mitsubishi Electric

At the SPS/IPC/DRIVES 2011 in Nuremberg, Mitsubishi Electric has presented a production cell with an integrated RH-3SDHR industrial SCARA robot for use in the pharmaceutical and medical industries. The application is designed for handling single-use syringes by removing them from the production conveyor belt for further processing after filling.

2012-01-18 – Next generation of development engineers use industrial robots from Mitsubishi Electric at WorldSkills

31 compact RV-2SDB industrial robots from Mitsubishi Electric were put through their paces at the recent WorldSkills international skills event held in London. Integrated into modular production systems (MPS) from Festo Didactic.

*Anmärkning: Texter och bilder är copyrightskyddade av Mitsubishi Electric. De kan användas fritt så länge de används för att rapportera och informera om Mitsubishi Electric och våra produkter. Användning av de här texterna och bilderna utanför press och radio kräver vårt uttryckliga samtycke.

Förfrågningar
Kontakt
Kunskapsdatabas
Hjälp