• Registrering
  • Login


Print page

Drivenheter & Rörelse

Få tillgång till originalkällor

Senaste nytt

2017-11-28 – Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages

Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.

Drivenheter & Rörelse

2017-05-05 – Key technology supporting packaging applications on their journey to Industry 4.0

Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017.

2017-03-23 – Mitsubishi Electric adds advanced condition monitoring capabilities to the FR-A800-E inverter series

Mitsubishi Electric has extended the diagnostics capabilities of variable speed drives by integrating smart condition monitoring (SCM) technology in a new version of the FR-A800 inverter series. With the new FR-A800-E line, the company has advanced the concept of drive-based condition monitoring. The user is able to carry out condition monitoring functions directly within the inverter.

2017-01-10 – Web server functionality and 100Mbit Ethernet interface available with Mitsubishi Electric Inverter FR-A800-E

Mitsubishi Electric is set to launch the latest addition to its FR-A800 inverter drives in Europe this year. It is based on its FR-A800 series variable speed drives with an integrated web server and 100Mbit Ethernet TCP/IP connectivity as standard.

2016-10-31 – Solutions for Industry 4.0 presented by Mitsubishi Electric at SPS IPC Drives 2016

At the forthcoming SPS IPC Drives Expo Mitsubishi Electric is showcasing a portfolio of integrated automation components and services developed to help customers realise their individual business objectives. Visitors to this year’s booth can explore new application solutions that enable the automation and digitalization of industrial processes and also exchange ideas ...

2016-06-08 – The future of inverter drives in the water industry

The challenges facing the water industry include climate change, rising energy costs, tightening legislation, population growth and increasing usage per head. The use of automated systems in order to make pumps and processes work more efficiently is helping keep pace with these demands; however, what does the future hold for one ...

2016-04-28 – Mitsubishi Electric's iQ Platform and Standard PLC Open Function Blocks reduce time to market for packaging machines

Mitsubishi Electric will be using a tubular bag machine to demonstrate its packaging machine engineering expertise at Hanover Trade Fair. The trade fair application is based on Mitsubishi Electric's automation iQ Platform. The system uses predefined function blocks especially for packaging machines which can be used to set up control systems including HMIs quickly and easily. The program ...

2016-03-17 – New - Mitsubishi Electric powered Delta robots from Codian Robotics

Mitsubishi Electric’s popular MELFA range of compact SCARA and articulated arm robots has been effectively extended by the introduction of new Delta style robots from well-known manufacturer Codian Robotics. Employing high precision servo motion technology and easy to use software from Mitsubishi Electric the new range is fast, precise and user friendly. Ideal for lightweight pick-and-place...

2016-03-08 – Mitsubishi Electric announces a significant presence at UK Drives & Controls fair, 2016

UK trade shows have experienced their ups and downs over the last two or three decades, however, they have endured and are now enjoying somewhat of a resurgence in popularity as exhibition organisers and venues work together to improve the relevance and accessibility of their events. Against this backdrop Mitsubishi Electric has committed to take a large space at the 2016 Drives & Controls ...

2015-11-27 – New medium voltage inverter meets the challenges of today with the technology of tomorrow

Mitsubishi Electric are launching a range of innovative medium voltage inverter drives at SPS IPC Drives 2015 (Nuremberg 24-26 November 2015), which are designed for both the current and future energy needs of industry. The drives are compact and modular, allowing for flexible installation in confined areas and deliver industry-leading energy efficiency with advanced IGBTs ...

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-11-17 – New inverter brings reliability, intelligence and cost saving to pump, fan and compressor operations

False alarms and unnecessary service trips due to shut down of pumps and fans are increasingly unacceptable as industry strives for greater operational efficiency and plant availability. The new FR-F800 inverter drive from Mitsubishi Electric provides an intelligent solution to this emerging need and represents the next generation of speed control for general purpose pumps, fans and compressors.

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-04-16 – Mitsubishi Electric and partners demonstrate hands-on handling solutions

At this year's Hannover Messe, Mitsubishi Electric and partners will be presenting hands-on handling and automation solutions. The focus will be on robotics including an integrated high-precision, flexible laser marking solution from Taufenbach GmbH, an automated screw application system from WSM-Automation GmbH, an application from Bilfinger HSG and Datalogic S.R.L. ...

2015-04-02 – Preview - Solutions for the water industry at the "PUMPENplatz"

Mitsubishi Electric will be presenting an innovative portfolio of solutions designed specially for the water industry at the "PUMPENplatz" at Hanover trade fair on Stand G43, Hall 15. Providing consumers with clean drinking water is a vital process but handling waste water correctly is also an extremely critical issue. Strict requirements such as the Urban Waste Water Treatment Directive provide..

2014-11-28 – IP55 variant added to FR-A800 series of frequency inverters

Mitsubishi Electric has added dust and splash-proof versions with an IP55 protection rating to its FR-A800 series of modern frequency inverters. Specially designed for harsh environments, the drives are highly robust and ideally suited for use in industrial and commercial building automation systems as well as in heating, ventilation and air-conditioning systems.

2014-11-27 – Energy Assist Unit from Mitsubishi Electric uses energy feedback and reduces energy peaks

At this year's SPS IPC Drives, Mitsubishi Electric will be presenting the Energy Assist Unit for the first time, a particularly effective intelligent solution for feeding regenerative energy from servomotors over 30 kilowatts back into the system so that it can be made usable again and ultimately reduce energy peaks significantly. This is the ideal solution for tapping into the energy and cost-sav

2014-11-11 – Regenerative energy, reduction of energy peaks and innovative products – the highlights at SPS IPC Drives

Visitors to the Mitsubishi Electric stand 380 in hall 7 at this year's SPS IPC Drives can expect to see a range of innovative factory automation products based on Industry 4.0. The highlights will include the Energy Assist Unit, the MR-J4-TM servo controller and the new GS series HMIs.

2014-10-20 – Mitsubishi Electric Servo controls pressure control for material determination

At this year's Motek trade fair, Mitsubishi Electric demonstrated a new handling application with pressure control directly controlled by servo amplifiers. The demo application showcased a number of innovative features developed by Mitsubishi Electric, including third-party motor control, high-precision direct-drive motors which interacted with robots and third-party motors, PLC CPUs ...

2014-09-29 – Energy from Waste sector gets ready for expansion and development

Mitsubishi Electric’s first-time presence in the EfW (Energy from Waste) hall at the Resource Efficiency and Waste Management show (RWM) in Birmingham, UK, has been hailed as an immediate success.

2014-04-22 – Preview components 2014 - Mitsubishi Electric Europe and Robotronic exhibit world’s first syringe handling solution with a small footprint

At this year’s components show, which is being staged in parallel with interpack, Mitsubishi Electric Europe and Swiss robotics specialist Robotronic are jointly presenting a brand new handling solution for supplying pre-filled syringes to an end-of-line packing system. The unique concept takes up very little space, yet offers a high processing rate of up to 600 syringes per minute and ...

2014-03-12 – IFAT preview - Mitsubishi Electric designs special water management solutions

At this year’s IFAT – the world’s leading trade fair for water, sewage, waste and raw materials management – Mitsubishi Electric, along with its subsidiary ME-Automation Projects GmbH (formerly KH-Automation Projects), will be presenting a range of innovative solutions designed for the water market. The two companies will be sharing Stand A5 425/524 in Hall 5.

2013-11-26 – New FR-A770 690V frequency inverters: high performance in harsh environments

The new FR-A770 inverters – high-performance devices with an operating voltage of 690 volts – are Mitsubishi Electric’s latest additions to the tried and tested FR-A700 series. The FR-A770 inverters are based on the successful FR-A740-EC models and are ideally suited for use in harsh environments.

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-26 – New FR-A800 series of frequency inverters provides maximum drive performance for plant and machinery

One of the highlights on the Mitsubishi Electric stand at this year’s SPS IPC Drives will be the new-generation FR-A800 inverters. The ultramodern drive has been specially designed for use in classic plant and machinery and with its maximum output and performance, increased efficiency and productivity are guaranteed...

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-06-10 – Award recognizes Mitsubishi Electric MR-J4 servo as ‘giant leap forward in precision motion’

Mitsubishi Electric’s latest MR-J4 series of servo amplifiers has won a prestigious ‘Product of the Year’ award in the Motors, Drives and Motion product category of the annual industry awards organised by respected European industry title Control Engineering Czech.

2013-05-29 – Mitsubishi Electric programming software and Simple Motion Modules certified compliant with PLCopen standard

Mitsubishi Electric Europe has been awarded a Certificate of Compliance for Function Blocks for Motion Control by PLCopen for its Simple Motion Module and GX Works2 software. The certification recognises the compliance of these products with IEC61131-3 standards in implementation of motion control function blocks, and demonstrates Mitsubishi Electric’s commitment to best practice in automation...

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2013-04-15 – Energy Efficiency with Mitsubishi Electric and KH-Automation at WASSER BERLIN 2013

At the WASSER BERLIN INTERNATIONAL Show from 23 – 26 April 2013, Mitsubishi Electric and KH-Automation Projects will present automation solutions for the water sector. The two companies specialise in systems for the water, waste water and waste materials sectors. The focal points are energy efficiency, remote maintenance, preventative maintenance and condition monitoring.

2013-03-05 – Smart conveyor lines up quiches for precision baking

In the drive to reduce packaging and its resultant waste, a specialist machinery builder has developed a pressureless queuing conveyor for collating quiches prior to baking.

2013-02-13 – Mitsubishi Electric optimises Irish waste water treatment and purification plants in record time

The aim of the operators of a waste water treatment plant and four associated purification plants in the East of Ireland was to reduce ongoing operating costs through modernisation. In order to do that, the plant was brought right up-to-date by installing Mitsubishi Electric automation components. This involved taking particularly diverse performance requirements into account as well as ...

2013-02-12 – Optimum servo system parameterisation with just one click - “One-touch tuning” with the MELSERVO MR-J4 amplifier series

Mitsubishi Electric sees the Fachpressetage Stutensee in Karlsruhe (5-7 February 2013) as the perfect opportunity to present its new MELSERVO MR-J4 amplifier series with “one-touch tuning” function. Compared to the previous series, the MR-J4 series simplifies operation and commissioning once again while ensuring a high level of performance at the same time. The result: increased safety ...

2012-12-04 – MELSERVO series now compatible with existing networks and numerous third-party motors

At this year’s SPS IPC Drives, Mitsubishi Electric supplemented its existing comprehensive servo and motion control portfolio with expanded network solutions supporting EtherNet/IP, PROFINET and EtherCAT for its tried and tested MELSERVO series.

2012-12-04 – Energy recovery in vertical lift system thanks to the latest inverter technology from Mitsubishi Electric

Mitsubishi Electric showcased energy-saving solutions on stand 380 hall 7 at this year’s SPS IPC Drives. One of the focal points is an exhibit that stands approximately five metres high and highlights the way a Hänel Lean-Lift® operates. The Hänel EcoDrive® lift system for intralogistics tasks uses the compact Mitsubishi Electric FR-A741 frequency inverter with integrated energy recovery function.

2012-12-04 – Combat rising energy costs with energy management systems from Mitsubishi Electric

Energy transition has resulted in an increase in energy costs and has made the subject of energy efficiency increasingly significant. The primary concerns of the production industry include the need to ensure that companies remain competitive, even with rising energy costs, and that production processes continue to run smoothly without any problems.

2012-10-23 – Mitsubishi F700 inverters now offer BACnet support for building services applications as standard

Mitsubishi Electric has upgraded the FR-F700-EC range of inverters with network support for BACnet, the most common data communications protocol in building automation and control networks. Introduced in 1987, BACnet is today the backbone of the vast majority of building services networks, and support for the protocol on the FR-F700-EC makes it easy to integrate the drive into building services.

2012-10-18 – Inverter enhances its solutions for of pump and water applications

Mitsubishi Electric has upgraded the FR-F700-EC range of inverters with a number of functions that meet the specific needs of water and pumping applications. The new functions supported by the upgrade include a pre-charge function, built-in PLC functionality, expandable I/O and a unit calculator for PID control.

2012-04-24 – MELSERVO MR-J4 – Innovative new technology for improved safety, productivity and energy efficiency

With the introduction of the new MELSERVO MR-J4 series - and corresponding positioning modules, motion modules and high-end motion control systems - Mitsubishi Electric is now offering a servo amplifier which will enable machine manufacturers and end customers to improve both safety within the production process and productivity, while guaranteeing ease of operation and commissioning at same time.

2012-01-04 – Mitsubishi Electric adds Ethercat Communications to its MELSERVO Servo Drives

Mitsubishi Electric’s MELSERVO MR-J3-A series servo drives can now be EtherCAT ready, with a new communications module that delivers increased speed and performance for demanding motion control and other automation applications.

2011-12-14 – Mitsubishi Electric makes motion control easy with the MELSEC L-Series Simple Motion Module

Mitsubishi Electric has expanded its MELSEC L-Series range of positioning modules with the new Simple Motion Module, enabling advanced motion control functions such as positioning, speed control, torque control, cam control, synchronous control and mark detection to be realised easily with just simple parameter settings and a sequence program accredited to IEC 6M3N-3 standard.

2011-10-18 – New 7kW and 9kW motors from Mitsubishi Electric complete high performance servo range

Mitsubishi Electric has added two new models to its HF-JP series of high speed, low inertia motors designed for demanding machine applications. The new 7kW and 9kW models complete the HF-JP range, which now extends from 500W up to 15kW, providing engineers with the ideal motors for building compact, high efficiency, high speed machines.

2011-04-13 – Mitsubishi Electric marks 30 years of success in variable speed drives

With over 30 years of expertise in variable speed drives development, there are few companies better placed than Mitsubishi Electric to translate market requirements into effective solutions or to drive trends in motor control. The company has sold more than 14 million frequency inverters worldwide, reflecting the quality of the products and the trust that customers place in the company.

2011-03-31 – Powerful, compact inverter from Mitsubishi Electric offers safety as standard

Mitsubishi Electric has introduced a next generation compact inverter that takes the concept of integrated safety to the next level. The successor to the popular FR-E700 inverter, the new FR-E700SC-EC provides the same power and versatility but with upgraded safety functionality, including integrated Safe Torque Off (STO) functionality and a new safety terminal block.

*Anmärkning: Texter och bilder är copyrightskyddade av Mitsubishi Electric. De kan användas fritt så länge de används för att rapportera och informera om Mitsubishi Electric och våra produkter. Användning av de här texterna och bilderna utanför press och radio kräver vårt uttryckliga samtycke.